This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53355 WEBENCH Cvdd VDC value

I think Cvdd value is fixed 4.7uF, 10VDC at the start. This value is the same when Vin is 12V too. In this case, it is over VDC value, so I think Cvdd's VDC rating should change depend on input voltage.

Best Regards,

Kohei Sasaki