I tried setting the Hi-side FET and low-side FET to be FDMC7572S into the LM2743 circuit (“custom FET” in edit mode) by entering properties of the FET into the WeBench. Maybe I’m doing something wrong, but I could not find a way to simulate the circuit with the custom FETs (i.e. determining Op Vals). Should I be able to generate the Op Vals after I change the FETs? If so, can you tell me how?