This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LME49710 Tina/PSpice model problem

 Hi,

I found a problem in LME49710's spice model in Tina and PSpice.

The main problem is that supply current is fixed at 4.8mA, even during operation.

For example with a output sinewave of 10Vpeak on 1kohm (10mA output peak current), the power supply current remains 4.8mA costant.

This make impossible to use LME49710 like the App Note SBOA009, for example.

Do you have any updated model without this problem? Or an advice to modify the original one?

Thank you Best regards

Federico, from Italy