When set up in Webench for VIN 11.4>12.6, VOUT = 0.90V, IOUT = 10.5A, COUT is selected as 330uF. If I edit COUT, the upper limit is shown to be 419uF. The datasheet does not specify a COUT MAX, and pg 20 states use of 560uF to handle transients.
Why is Webench not allowing a COUT > 330uF? How can I edit the design to use, let's say, a 470uF cap and two 10uF caps in parallel = 490uF?
~Leonard
GDCanada_LM2743_11Vto0V9_10A[wc].pdf