Hello,
There are times when the voltage value and current value of the signal source that is not connected a voltmeter and ammeter is displayed in the graph.
It is also when it does not appear.
What changes data displayed?
Voltage and current of signal source without the voltage meter and ammeter is displayed. TRIAC_ACST610-8_gnd_no.TSC
Only voltage that connects the voltage meter is displayed on the graph. TRIAC_ACST610-8_up_gnd_no.TSC
Kechan,
2055.TRIAC_ACST610-8_up_gnd_no.TSC