This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH schematic not working eagle possible lib problem

Hi. I used webench to design a switcher. see attached zip file. I think there is a problem with the library. I could not get the schematic or the board to open. I have attached both. Any help would be great. I noticed that Cin doesn't have a foot print in the bom. that may be the problem. but I don't see why that would prevent the schematic from opening.

I also saw in this forum that frequently the problem is with the library file. but I didn't see how to solve problems with the library if you can't get the files to open at all.

Any help appreciated.schematic_3637586_56_Eagle.zipboard_3637586_56_Eagle.zip