Other Parts Discussed in Thread: TINA-TI, LP2992
We need TINA TI compatible library or Webench support for below parts to plot its transient response: -
- TLV1117LV12DCYT- 1.2V Regulator
- LP2992IM5-2.5/NOPB- 2.5V Regulator
- LP2992IM5-1.8/NOPB- 1.8V Regulator
On ti website SPICE library is available but I am not able to import them in TINA TI due to library incompatibility. If I try PSPICE to simulate it than I am stuck with .slb file which is not provided in the library file available on ti website.
Kindly look into this and see if either TINA-TI compatible library can be provided or either webench support for these parts which could aid our analysis.