This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC1614 / WEBENCH Designer for Inductive Sensing Applications: Axial position sensing

Guru 29720 points

Hi Team,

I simulated to design LDC in WEBENCH and consider to export CAD file.
I would like to select 4 layers PCB solution.

By the way, is there any restriction about the thickness of layers?
Do I have to consider the thickness of layers to design LDC?

Best Regards,
Yaita

  • Dear Yaita,

    You can select a 4 layer PCB solution from the solution list as shown below by selecting a solution with an entry of 4 in the "layers" column. The assumption for thickness made here is 1 OZ copper thickness. Please let us know if that doesn't answer your questions.

    Regards,
    Shrikrishna,
    Texas Instruments.