This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55340 / IC Tj limit

Other Parts Discussed in Thread: TPS55340

Hi Everyone,

I tried to simulate with following setting but the error was occurred.

  • Vin = 2.8V - 4.0V
  • Vout = 7V
  • Iout = 1.5A

 

I reduced output current and then the simulation was successed at 1.43A with IC Tj = 84.9C. I increased the output current to 1.44A then the error was occurred. So I guess that the IC Tj is limited at 85C. Tj(max) should be 150C so please check setting of Webench.

 TPS55340_Vin=2.8 to 4.0V_Vout=7V_Iout=1.42A.pdf

Best Regards,

Sonoki / Japan Disty

  • Hi Sonoki,

    If you input the below specs and " Click why devices were not found" in the visualizer and or choose it from the pop up that comes up. Filter for TPS55340 and you will notice that the device hits current limit with this spec. It's not a temperature issue. The TjMax for this one is correctly set at 150C.

    • Vin = 2.8V - 4.0V
    • Vout = 7V
    • Iout = 1.5A

    Please let us know if you have any concerns still.

     

    Regards,

    Pavani Jella

    WEBENCH Applications