Other Parts Discussed in Thread: TINA-TI, UA741, OPA277
Would someone please review this simple op-amp circuit, which should be a non-inverting Schmitt trigger, but which TINA-TI is showing as an inverting amplifier: http://img42.imageshack.us/img42/4968/nonamerc.jpg
The basic circuit is taken from Wikipedia at http://en.wikipedia.org/wiki/Operational_amplifier_applications#Schmitt_trigger . Nominal values were selected for R1=R2=20 kOhms, and Vcc = +/- 10V. Input to the circuit is a 5 kHz sine wave with amplitude of +/-4 V. TINA shows the circuit has an output exactly equal to the negative of the input, which is not expected.
Thanks,
Mike