Other Parts Discussed in Thread: LMR62421
Hello,
I'm about to use the LMR62421 boost regulator for boosting from 3.0V-5.5V to 16V with max. 0.2A output current. When I try to simulate the design using Webench I get following message
When I click the green button "Show Why Parts Were Not Found" I get following screen saying that design is not stable and the calculator cannot create the design.
Does it mean that the Calculator has some limitations or the circuit cannot be made working? I've designed the converter with this chip "manually" using datasheet and I don't see any reason why it should not work.
Please help me understand the Webench behavior.
Best Regards,
Josef Rypar