Other Parts Discussed in Thread: TPS2511, TINA-TI, TPS2546
Hello,
I am trying to do the simulation of the TPS2511 in TINA9-TI but it seems that the file is encrypted. It is possible to have the model decrypted?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Pedro,
Yes, it is possible, but you will need an NDA for the unencrypted model. Please refer to the following post. There is a section in this post that describes how you can get the unencrypted models.

Thanks,
Hi Pedro,
Alternately, if you are open to using another device, you could use TPS2546 which has a TINA-TI model available.

Thanks,
Hello Nikhil,
The TPS2511 is the ideal component to the solution I need.
The purpose of the TPS2511 Pspice model would be to test different combinations of resistors (relatively to the feedback pin of the buck regulator and the CS pin of the TPS2511) to compensate the voltage drop in the USB cable.
I already have an idea of the resistors values but I would like to test different scenarios.
Thank you for your help.
Pedro