Other Parts Discussed in Thread: TINA-TI, TPS54478, TPS56121
A few questions:
- Can I make it use all 4 cores? On my quad core PC is uses exactly 50% CPU only (although it seems to use 20-80% of all 8 virtual cores, not 100% of some and 0% of some).
- Can I terminate without losing the data so far?
- The result can only be saved as a TDR file. Can I open this later? Tina-TI doesn't want to open it.
- Should I set time step manually or is that automatic?
- Can I change the library into which it dumps "autosave" files?
- If I open one schematic, simulate for an hour, save as TDR, then open a different schematic, simulate for an hour, save, then it overwrites the old file without prompting. It should base name on schematic, and prompt before overwriting.
- For the TPS54478 average model instructions say that if L1 is to be changed then please change it both in the macro and L1. L1 says 1.2uH 20mohms but if i right click and select "Enter Macro" it says 1uH and 10mohms. Shouldn't those be the same?
- And if I choose "Enter Macro" for the PWM circuit and change 1000K to 800K, it doesn't remember what I wrote (I chose "Save as" that was the only way to save it I could find)
- The only help file I find has no help on the above subjects. Did I miss something? Webench and LTspice are easier to use and have more help.
Best regards
David