I'm designing a buck system using TPS40304. When input and output are given, an automatically circuit will be generated and I can see these functions as the Fig1 below.
However, after I modified some of those components, I can only see these functions as Fig2. Where are the left gone and how can I judge the loop stability of the whole system?