Hi there,
I am using EasyPLL to update an old design using LMX2330L and ZComm V630ME09. As the specific VCO is not in the library, I have to input the parameters manually. The loop filter is created OK, but lock time graphs and spurs analysis results are not shown. The graph's axes are shown, but with no trace. When using a listed VCO the problem disappears. I see two other posts from more than a year ago describing similar issues. Could it be as a result of the custom VCO parameters?
Francois