My apologies if this is not the correct place to post this but i am looking to use the TI USB to GPIO converter just to control the logic on the output pins (no PMBus, SMBus or I2C). Should this be possible with the packaged software or does it need a slave board? When i have connected it up and successfully installed the USB driver it still says 'Adapter not attached'
Any help would be greatly appreciated