Other Parts Discussed in Thread: TINA-TI
Sorry to pop a 2 in 1, hope it's ok.
Recently I wanted to simulate circuits with thyristors, but can't find them or any mention to them inside TINA. Are they hidden somewhere? I'm guessing there is a full version of TINA or something like that.
I also came across a reference about doing interactive analysis in TINA, but failed to get it done. As an exemple, I wanted to simulate a Latch-On circuit with 2 transistors using a button On-Off for the trigger. In the end, I used a switch with the timer function combined with the transiente analysis (works perfect), but wanted to know if I can manually press buttons and watch the changes immediately reflected on the results (with the interactive analysis). Maybe this is also a feature in a complete version of TINA?
Thank you!