Other Parts Discussed in Thread: TINA-TI
Hi,
I'm referring to the Figgure 3 from the below app note. However, in TINA simulation, it reports 'convergence problem'. Could you help analyze the reason?I've uploaded the TINA file.
Thanks.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TINA-TI
Hi,
I'm referring to the Figgure 3 from the below app note. However, in TINA simulation, it reports 'convergence problem'. Could you help analyze the reason?I've uploaded the TINA file.
Thanks.

Hi Di Wang,
I was able to resolve your Convergence problem (which I also observed) in TINA-TI by selecting Analysis, Set Analysis Parameters, Shunt Conductance (S)= 100m (was originally 0).
In addition, in the same panel, I was able to improve Step response shape by changing "TR Excitation Subdivisions" to 1000 (was 10).
Here is the Transient simulation:
Here is your new TINA-TI simulation file with these changes incorporated:
LM6172 E2E Convergence Issue resolved Hooman 8_27_15.TSC
Regards,
Hooman
Di Wang,
There were a few issues with your circuit that may also need to be fixed. R13 should be 10k, not 0. R12 and R11 should both be 3.9k per the schematic. The connection from C5 to D2 should be removed. After these corrections, the circuit still did not function as it was supposed to. I did vary a few of the simulation parameters and the input source and actually got the -10V output that was expected.
I changed a few other items as well to clean up the schematic. The circuit is still very fragile in terms of convergence, so you may have to tune it further if you make any further changes.