Hello! I have been using the WEBENCH tool to design buck converters and would like to export the cad file directly to Altium. Every design that I have exported, I have also selected to include the 'footprint' for every componnent that is inside the design and the BOM.
There is a problem though when importing the library into Altium through the 'readme'. When the library is created, the only components that are being imported into Altium and are available to select inside the library are the converters, and half of the capacitors. Inductors and resistors are not being included in the library. A quick note for all components is, they are all surface mount.
What steps am I going over when properly importing or is there another way to make sure every component is getting fed into Altium?