Other Parts Discussed in Thread: SN74AUP1G97
Hello, I want to simulate the SN74AUP1G97 ibis file.
I have imported the ibis file into ADS & Pspice, however, there are only 4 pins in symbol not a 6 pins.
If other 2 pins are already connected to ground and Vcc each, how can I connect 4 pins to use as an inverter in datasheet?
4 pins' name are not A,B,C,Y like as datasheet but In, PC, GC, DigO in ibis symbol.
I will give 3.3V squre wave for input signal with 5n sec rise, fall time. So I want to see inverted output signal for 1MHz~10MHz frequency sweep.
Thanks in advance! :-)