Other Parts Discussed in Thread: LM5111
Hello,
I try to run a simulation in LTspice in order to test my design with the LM5111-1 Dual 5A Compound Gate Driver, driving a Infineon IPT004N03L.
However, I encounter a problem whenever the VEE port of the LM5111 is not directly connected to the ground node of LTspice. I created a simplified model that clearly shows the difference between a working and a non working circuit (see below/attached). I think some of the subcircuits within the LM5111-1 spice model are connected directly to node 0 (spice ground) instead of VEE, which is problematic if VEE is not connected to Ground/Node 0.
I tried to replace all " 0 " connections with " VEE " but spice threw an error: "Singular matrix: check node u2:_u11:vee Iteration No. 1"
The model I used in the example can be found here: www.ti.com/.../snvmad2
I also tried the other models of LM5111-1: www.ti.com/.../toolssoftware
Since the control voltage is not directly connected to ground but isolated in my design, the model doesn't work for me, I think? Is there a solution tto make it work or do you think I made a mistake in using or importing the model?
Thank you in advance,
Matthias
P.S.: Using LTspice 4.23h on a Windows 7 Enterprise 64bit
--------
Screenshot & zip file with LTspice circuit, Plot and LM5111-1 model