Hi,
I was working in the Lm2678-5V buck converter and happened to not find an low-esr capacitors around. So here are my doubts:-
- Is it okay to use Ordinary ESR capacitors with the same capacitance rating(or should I increase the value) and whats are the performance setbacks I should take into account if so due to ESR rating?
- Is it okay to use capacitors with higher capacitance rating (ESR and Non-ESR) than specified in the Webbench Simulations?
- Will higher capacitance and ordinary ESR affect anything other than the Turn ON time(due to time take to charge in the input and output capacitors)??
- About the di/dt loops in the PCB board, how does it affect if I use a number of Input and Output caps in parallel ( to increase the capacitance) do?