Hi,
I get an System exception if I select B.O.M. or want to print my design with the checkbox B.O.M. checked. Is this a problem with the new version ?
Andreas
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I get an System exception if I select B.O.M. or want to print my design with the checkbox B.O.M. checked. Is this a problem with the new version ?
Andreas
Hi Andreas,
We are able to reproduce this issue. It affects old designs for certain parts. If you create a new design with same inputs, you will not get an exception. Which part was this design for?
Thank you for reporting this.
Hetal.
There is an update coming out to fix this bug ASAP.
In the mean time, try this work around. It has worked for me. When you open the design that has the problem. Go to the "Edit Inputs" button. From there change just one character in the design name. Make sure the check box at the bottom of the form is left unchecked. Now hit the apply changes button. The bug is magically fixed because SwitcherPro updates the compensation resistors to newer versions of the same parts. These newer versions have a corrected tolerance parameter and they show up fine on the BOM.
Good Luck
Hello,
We released a hot fix for this issue. The new version is v3.7.8. Thank you for reporting this.
Hetal.