Other Parts Discussed in Thread: TINA-TI
ANALYSIS -> TRANSIENT shows a good looking output however it is only 5mV peak to peak.
It should match input signal which is 2V peak to peak.
TPL7407L TINA-TI Reference Design
Help please.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TINA-TI
ANALYSIS -> TRANSIENT shows a good looking output however it is only 5mV peak to peak.
It should match input signal which is 2V peak to peak.
TPL7407L TINA-TI Reference Design
Help please.
Ron,
The input source (VG1) is a 1.5V square wave that is fed into a voltage controlled voltage source offset by 1.5V and inverted (-1 for the gain) which becomes a 0V to 3V input to the device. VCOM is set to 24V, so all of the outputs are pulled to 24V.
Here are the simulation results:
I do not see a 5mv peak to peak output simulation or any 2V input peak to peak input signal.
Could you upload the simulation results (picture)? I am using the .TSC file that was attached to the message.
Ron,
You must be using a different .TSC file. Here is the one I was using.
You are using an older version of TINA-TI (you can update it from the web), but the default transient analysis window is very different than the one with the .TSC file you attached. I do not have a VIN or VOUT signal in the .TSC file that was posted.