This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Simulating LM2596 using webench, cant find solution to match the requirements.

Other Parts Discussed in Thread: LM2596

Hi,

I'm trying to simulate the LM2596 adj as a buck converter before attempting to work on my final project which is a 9V buck converter with varying inputs from 15V to 37V and 1.33A current but when i tried to input my design parameters on LM2596 interactive design I am faced with the following error:

"We're sorry, we could not find a solution to match these requirements. Please check to make sure your inputs are within the correct corresponding range. "

I don't know why webench can't simulate my desired parameters but when i tried to change the output voltage to 4V with the same input voltage of 15V to 37V and current of 1.33A, It gives me the correct design and simulation for 4V output. 

What could be the issue for this and any suggestion on how can i fix this error?

Thanks for your help