Other Parts Discussed in Thread: LMR14203, LMR14206
I question whether the webbench model for the LMR14203 is accurate. it fails when trying to use it for a design which the literature shows as typical. it errors as failing min TOn time. there should be no problem with min on time with the typical example. I was initially checking the part out with: 10-30 VDC in 3.3 VDC @0.075 A out when using webbench for the parameters above it allows the LMR14206 which is nearly identical. frequency is slightly different and it has a greater current capacity. ]
[Steps Needed to Recreate Problem:
model the parameters:
4.5-42 vdc in
3.3 vdc @ 300ma out.