Other Parts Discussed in Thread: CSD87502Q2
Dear Sirs or Madame:
I need assistance matching a MOSFET gate driver to a MOSFET. In simplistic terms I would like to turn a light on and off at a 1 to 3 Mhz frequency. The test MOSFET that I have is a logic level MOSFET that is capable of passing 35A and operate up to 100V. I would like to use a MOSFET with the same parameters coupled with a gate driver instead. I have been studying everything I can about gate drivers, but haven't really found anything that matches the driver to the mosfet. I am coupling my circuit for low side switching, would like a CMOS (vs TTL, but read there are other forms like F as well. I open to suggestions), my power supply for my test circuit is 12V, 1 amp. For testing purposes I am using a 555 timer with an RC couple to control the frequency.
Is there any help you can provide to get me to the right pairing of the MOSFET and driver?
Thank you very much for your help! :)
Tina