Hi,
I want to calculate phase margin and cross over frequency ... for the TPS54040.
If I use the WEBENCH design center and the TPS54040 Pspice average model in order to compute the Bode plot.
There is some small differences between the 2 tools:
For example :10 kHz of gap for the cross over frequency.
Who have right ? Is it due to the LC necessary to inject the AC signal on the PSPICE model ?
Thanks for your help !