This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS78233 - Load Transient Simulation in Webbench



I'd like to look at the load transient response of the TPS78233 for a design prior to doing my first build.  The results I was seeing in Webbench were a little too good to believe so I did a quick spot check against the condition shown in the datasheet.  

Datasheet conditions:

Vin = 5.5V, Vout=3.3V, Iout 0mA=>10mA for 10mS, Cout = 10uF

The above conditions in Webbench show an output droop of only ~1mV whereas the datasheet shows around 100mV.

Is there something I'm doing wrong? Are the results of the load transient sims in Webbench not accurate?