This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61175 Simulations

Other Parts Discussed in Thread: TPS61175, TINA-TI

HI,

I am using TPS61175 in my deisgn and also doing TINA simulations for the same.

I have provided input of 4V & my desired output is 30v / 300mA min

Here in simulations, if i need to generate 30v output, my load current need to be limited to 240 to 260mA...

Please confirm . I didn't changed anything in the TI provided TINA deck apart from the feedback resistor values for generating 30V.

Rset connected to freq pin is 51k , Soft start pin connected to 1nf.

Thanks & Regards

Jones