Other Parts Discussed in Thread: SM72295, TIDA-00120
Hello all,
I was wondering if it is possible to use this charge controller with a 31.45V,7.98A 250Watt panel for a 12 volt battery system?
I read the test report and saw that a voltage of 30VDC was being used for a 24 volt system. But would it be safe and compatible with a 12 volt system?
Also as far as the the charge controller goes, will it be able to determine how much life a battery has left?
Thanks,