This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Webench current limit with external switches?

Other Parts Discussed in Thread: LM5022, LM5122

I'm trying to simulate a white LED supply circuit with Webench. I'm shooting for 24V to 55V @ 5.6A output max. So far so good but Webench starts complaining LM5022 is limited to 15A.. 

As far as I can tell, LM5022 is a pure external switch design that has no provision at all to determine inductor current beyond what you feed into the current sense from switch source. So why this limitation? Can we have it lifted/modified? 

Also the datasheet has no mention of any current limit beyond the cycle-by-cycle CMC limit.