Hi,
I am new to circuit design and am trying to implementing a circuit suggested by webench using the TPS61088RHLT DC-DC Switching Boost Regulator. It's to step up a single cell lithium ion battery to a constant 9V, powering a IR LED at 0.5 Amps. I have very limited space on my pcb and was surprised to find that webench selected a "huge" 1206 package for the frequency setting "Rt" resistor, (249kohm), dimensioned to dissipate 250mW at up to 200V. Similar situation for the current limiting resistor RIlim.
Given that there won't be ever more than 9V in the circuit, the current through these high ohmage resistors must be negligible and the power dissipation well below 63 mW - so why does webench not select a 0402 package, like it does for most of the other resistors? Is this a mistake or am I missing something?
If webench does such over-dimensioning for the resistors, does that mean I can't trust the capacitor selection either and we might possibly get away with much smaller packages there as well?
thanks,
Stefan