This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

No suitable MOSFET

Hello, 
I have a problem with the provided high-end MOSFETs or rather the lack of thereof. I'm trying to create a 24V to 55V @ 5.6A boost converter. You have no suitable FETs for such. I have identified at few suitable candidates for this: 

100V 30A NXP BUK7Y38-100E 
150V 33A Infineon BSC360N15NS3
100V 40A Infineon BSC265N10LSFGA
100V 40A ST Micro STL40N10F7
100V 30A ST Micro STD30N10F7

And so forth, these are relatively inexpensive pieces. There's another discussion about webench current limits but even with reduced current output I'd need a pretty hefty MOSFET.