Other Parts Discussed in Thread: TINA-TI
I am designing an analog filter that has an inductor in it. Let's say it is 1mH. Does Tina model it as 1mH regardless of frequency?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
David,
Yes, unless you have a .SUBCKT model that can change the inductance value with the frequency of the signal applied. The simple inductor in TINA-TI will allow you an inductance value, Rseries value, Initial DC current, linear and quadratic Temp co, and maximum ratings for current and voltage.
There are a couple of non-linear inductors that can be used as well, and they allow some different parameters and cores to be chosen. You can use the Component Help in TINA-TI to give more details about their parameters and usage.