Dear Support,
I bought the TPS43060EVM , and I tested it with VIN 24V, Vout = 40V and Iout= 1.6A. I see that the temperature reached by M1 M2 and IC in TPS43060EVM, is much lower than in my project. So I would like to compare the result of the TPS43060EVM project in the WEBENCH with my project. The problem is that the selection of M1,M2 is possible only in couple, and the TPS43060EVM uses the same MOSFET (the BSC123N08NS3G) that are not selectable in WEBENCH.
Can anybody send me the WEBENCH project of the TPS43060EVM, including the PCB layout to simulate the temperature profile too ?
Thanks
Paolo