This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8803

Other Parts Discussed in Thread: DRV8803

I am drive this relay driver with a Arm Cortex M0.   I am using one pin on this processor to control two ports.   The spec says it only drains 100 uA at 3.3 V.   I am using 5 V.   When I try to drive this relay driver it works sparatically and the voltage of the pin drops to 2.5 V with it being turn on high.   This voltage should be at 5 V or close to it.   Do I need to respin this board with each of the pins being connected separately.