I've download and simulated the pspice model for the TPS3700 and it appears that OUTA and OUTB are triggering at 1 volt higher than my design parameters.
My design parameter below:
Vmon=6v
Vov = 6.3
Vuv = 5.7
And I used the current going through the divider as 5uA.
I calculated the following resistor values:
R1=1.2meg
R2=8020
R3=76.19k
After simulating, OUTA goes from low to high at Vmon=6.7V, and OUTB goes high to low at Vmon=7.3V. Is there a 1 volt offset error in the simulation or are my calculations in error?