Other Parts Discussed in Thread: UCC28740, UCC28730, UCC28704, UCC24636, PMP11451
I tried to simulate a flyback converter in Webench for UCC28740 converter with the below specification. Input: 85-265 VAC @ 50 Hz, Output: 20V @ 3 Amps. When i entered the values to get the design file in webench and got a error state that it could not find the MosFET to meet the design. But the application note and develpement board used the above output with the Mosfet IPL60R299CP. Please let me how to add the model for the Mosfet to continue to simulation.
Refer the link for application note: http://www.ti.com/tool/pmp11451
Thanks