How do I change the switching frequency for the TPS53819A in the TINA simulation? I can see how to open up the macro, and I can edit the macro to change FREQ_SEL=1 (325KHz) to FREQ_SEL=4 (600KHz) but there is no option to "save". I can do a "save as" *.cir, but the switching frequency does not change.
Also, the macro has FREQ_SEL=1, but the adjacent comment has FREQ_SEL=2. FREQ_SEL=2 is correct since this corresponds to 425KHz, which agrees with the simulation. Shouldn't the comment reflect the same value as in the macro?