The subject IBIS model has only Typ PVT (it is missing Min and Max PVT).
We can’t run a full set of SI sims with only Typ. PVT - please provide a model including min/max PVT for the SN65LVDS33PW
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The subject IBIS model has only Typ PVT (it is missing Min and Max PVT).
We can’t run a full set of SI sims with only Typ. PVT - please provide a model including min/max PVT for the SN65LVDS33PW
Hi Steve,
Due to the age of this device, our tools are not compatible with the version of SPICE used.
As a result, we are unable to generate new models for this device.
Regards,
David Larkin
Webench Design Center