This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Recommendation for the boot application in light load

Other Parts Discussed in Thread: TPS61236P, TPS61086

Hi, everyone

My application is to use one high boost efficiency IC in light load.

Below show the details:

Input: 2.5V - 4.4V

Output: 5.2V  @ 200mA(mA)

              5.2V @ 100mA(Typ.)

Can you help to suggest one solution to me?

Best regards