I can not enter the esr value of a capacitor. According to informations that I get from internet, I added a resistor as series with capacitor instead of esr value. For example; if esr value is 200m ohm, I added a resistor(200m ohm) as series with capacitor. Actually, my main purpose is measure output impedance. Therefore, I added an ohmmeter to circuit. My measurement results are wrong because of esr resistors. If I delete esr resistors, I can observe approximately true graph.I want to ask two question.
1)How I enter esr value?
2)How I measure output impedance by using ohmmeter?