Other Parts Discussed in Thread: LMR14203, LM2841
Is this a bug in webench for some devices or are the values just more optimised?
For example, the inductor chosen by Webench for a LM2841 using parameters similar to the examples in the datasheet gives an inductor that is 10x larger than the datasheet, example 150uH vs 15uH. It does this for other similar devices like LMR14203 as well. I've not done the maths myself yet so won't comment on its accuracy just yet. Was curious if others are finding discrepancy between datasheet recommendations and webench designs.