I have a problem - I'm on the TI website made SMPS Design using WEBENCH® Designer / LM3478, calculate scheme and has exported calculation results in Eagle (TI exports calculated results in version 6.4). The scheme opens normally, but the file * .brd does not open . Throws error:
"Warning(s):
line 1: ignoring redefinition of number="49" in tag <layer>
line 1: ignoring redefinition of number="49" in tag <layer>
line 1: ignoring redefinition of number="49" in tag <layer>
line 1: ignoring redefinition of number="49" in tag <layer>
line 1: ignoring redefinition of number="21" in tag <layer>
Error:
line 1, column 16840: redefinition of name 'V' in tag <pad>"
It is not clear what he wants. Where to find the "line 1, column 16840"? I am using Eagle 7.2.0 FREE. Can you help me to open the file * .brd?
Furthermore, similar error obtained in other calculations. It seems that this system error WEBENCH® Designer - he incorrectly converts the data to a file * .brd. By the way, for a long time CADsoft EAGLE applies 7.6 version!LM3478MMXNOPB 3.0V-7.2V to 6.00V_1.0A SEPIC.rarLM3478MMXNOPB 3.0V-7.2V to 6.00V_1.0A SEPIC.rar