The model appears to work well, but it does not seem to be able to model Vout when Vin is removed. The voltage follows Vin even if large amounts of capacitance are used on Vout. It seems as if this model will not model the output properly as Vout should hold for a few msec at least. Is there a reason why the output does not “hold-up”? It seems as if the model has an issue accurately modeling this.
Please let me know if I am looking at this correctly.
Thanks for your help with this!
Richard Elmquist