This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Piecewise Linear Signal



    Hello,

    I built a circuit in Tin.I used Piecewise Linear Signal as input and a sinus signal as reference.

  I use an opamp as comparator in this circuit.But when I made AC Analysis I can not get correct comparator results.Also, when I made AC Analysis I can not piecewise linear input signal correctly.

   Could you help me why I can not get correct form of input piecewise linear signal?

   Regards,

  • Could you post your .TSC file for this example? Also, what are you trying to accomplish by running an AC analysis on a linear ramp? Typically, AC analysis is used to determine the frequency response of a circuit, not the response of a linear ramp. Lastly, why are you using an Op amp as a comparator instead of simply using a comparator?