This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Vout p-p calculations in Webench

Other Parts Discussed in Thread: LM25117

I have two very similar designs with only output caps' difference. However, the results showed the opposite direction from what I understand and what from the datasheet of LM25117 page 29. This may not make a lot difference to the design but really like to clear it out. Please help a little detail on how the Vout p-p is calculated in Webench. Thanks,

(1) Vout p-p 9.692 mV with one 560uF Cout.

Design : 4561043/372 LM25117PMHX/NOPB

LM25117PMHX/NOPB 22.0V-26.0V to 12.00V @ 10.0A

(2) Vout p-p 26.382 mV with one 560uF and two 47uF Cout.

Design : 4561043/423 LM25117PMHX/NOPB

LM25117PMHX/NOPB 22.0V-26.0V to 12.00V @ 10.0A