Hi,
I was showing to my colleague how to use WEBENCH designer.
So Selected an LM2678-ADJ in order to set-up a 7V output supply.
But we noticed if the input voltage is above 25V it gives-up with an error " The design cannot be created"!
If the max voltage is 25V or lower it works OK.
Am i missing something?
Is there an undocumented limitation?
In our example we selected Vin Min20V, Vin Max26, Vout 7V and Iout 1A.
Any comment?
Regards
Francesco cembrola