Using Webench power, I've done a few simulations no problem (e.g. TPS54561 48V in 12V 5A out) but I have noticed an issue with reports.
Thermal simulations work well, and display correctly, but when "printing" a report to PDF the operating conditions are incorrect if altered from the original design parameters. e.g. was originally designed for 5A out, but if simulated for 4A out the simulation results look fine, but the PDF report incorrectly lists the operating conditions as 5A which makes it very confusing to look at later on.